AXIS#.SAFEPARAM.SLI_#.TIMEDELAYMONITORING

Description

Indicates the delay before starting the position monitoring when the Safely Limited Increment (SLI) safety function is activated.

 

This value is t_D_SLI in diagram below:

Context

For complete SLI information refer to SLI (Safely Limited Increment).

Related safety parameters:

Versions

Action Version Notes

Implemented

02-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Milliseconds

Range

[0, 60000]
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
AXIS1.SAFEPARAM.SLI_1.TIMEDELAYMONITORING

3169h

04h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLI_2.TIMEDELAYMONITORING

316ah

04h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLI_3.TIMEDELAYMONITORING

316bh

04h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLI_1.TIMEDELAYMONITORING

3269h

04h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLI_2.TIMEDELAYMONITORING

326ah

04h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLI_3.TIMEDELAYMONITORING

326bh

04h

Unsigned16

-

-

Read/Write

No